2/2/2010 9:06 AM | |
Posts: 183 Rating: (8) |
Hello DanielMelo; |
2/2/2010 12:22 PM | |
Posts: 5 Rating: (0) |
I set the default configuration: time covered by a single segment 1 day, max size 100 Megabytes. I appreciate your attention with this matter. |
2/3/2010 6:59 PM | |
Posts: 5 Rating: (0) |
So Mr. JOTST, the CAS is down now and I still have the same behavior as before . I am using PCS7 V7.0 SP1. |
2/10/2010 11:25 PM | |
Joined: 5/18/2006 Last visit: 10/21/2020 Posts: 170 Rating: (63) |
See extract from PCS 7 Compendium. Even though Microsoft SQL permits larger segment sizes and number of segments performance starts to fall off if you exceed the recommendations as noted in the compendium. so make sure your archive config (all, alarm, tag fast and tag slow) combined meet these recommendations. Compendium Part A - Configuration Guidelines (07/2009, English) section/chapter Archive configuration for TagLogging Fast and TagLogging Slow
|
Follow us on