Industry Online Support
Technical Forum
2/11/2010 8:13 AM | |
Joined: 9/6/2008 Last visit: 3/29/2024 Posts: 134 Rating: (16) |
one way is to change the value of the timer block ( e.g b003 is delay on ) you pres esc due to run , then move to program >edit >select the block (b003 in this example ) >ok>with up and down move on the value and modify it>press ok and esc or choose the next one which you want to modify. of corse is not the easiest way . another way is to use the td panel, build a program with mesage texts that alow you to modify the timers with the f keys and is very easy and safer for your customer to make the changes. i atach a simple circuit just for to see how to work with it! or you can make a search at the forum and you will find many similar examples! Attachmentref.time from td.zip (402 Downloads) |
http://electrotech-techblogg.blogspot.gr/ |
|
2/11/2010 9:45 AM | |
Posts: 378 Rating: (47) |
Just for your interest. If you want to open cdrshort´s .zip-file you have to rename it to a .rar-file. best regards O_Moderator |
2/11/2010 3:31 PM | |
Posts: 89 Rating: (1) |
Thangs a lot |
Follow us on