12/16/2009 3:41 PM | |
Joined: 12/9/2009 Last visit: 4/18/2024 Posts: 156 Rating: (11) |
Hello, |
12/17/2009 3:30 PM | |
Joined: 12/9/2009 Last visit: 4/18/2024 Posts: 156 Rating: (11) |
Hello, the SOFTNET Security Client supports only one VPN tunnel. I understand right that you want to have further connections from the external network into the internal network of the SCALANCE S61x ??? There is possible to use a second PC with SOFTNET Security Client which establish a further VPN tunnel to the SCALNACE S61x. Or you use also a SCALANCE S61x on the side of the PC like in following example: http://support.automation.siemens.com/WW/view/en/24968211 The SCALANCE S61x supports more than one VPN tunnel |
Follow us on