Industry Online Support
Technical Forum
4/11/2010 10:45 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (306) |
Hi all We need to follow the attached drive control philosophy in one of our projects using CEMAT V7.0. We found the default standard "000" - Normal closest to our requirements and worked on that. However in this standard we cannot meet some of client's requirements e.g. Local control from individual drive faceplate. Is it possible to modify the default standard to suit our requirements, ir should we use a different standard to meet these specifications ? Thanks & Regards Navnag AttachmentControl_Philosophy.PDF (86 Downloads) |
There is no such thing as the last bug in a program |
|
Follow us on