Industry Online Support
Technical Forum
5/28/2010 6:12 PM | |
Posts: 4 Rating: (0) |
I have one question for you , which functional block i have to use for communicate with a PC (TCP communication)? And which address i have to register PORT address or PN/IO address? I used last time a CP343 and i used FC5(AG_SEND) and in field "LADDR" i write the address of the port. Here is the same? Thanks for your support
Splitted from CPU 315-2 PN/DP. |
Last edited by: O_Moderator at: 5/31/2010 9:26 AMnew subject after splitting |
|
5/28/2010 7:37 PM | |
Joined: 9/27/2006 Last visit: 5/10/2024 Posts: 12257 Rating: (2666) |
Hello James; It would be advisable to start a new thread when you want to recieve answers from the forum, the question you are asking has nothing to do with the title of the thread... Simply chose a conference (or any thread) and clink on the New Thread link at the bottonm of the page... That said, why dont you look at Ammy's reply in the following thread about communications in Step 7: /tf/WW/en/Posts/37702 I would suggest you use BSEND/BRCV functions to exchange your data over Industrial Ethernet. The online help of Step 7 should get you started on them. Hope this helps, Daniel Chartier |
5/29/2010 8:11 AM | |
Posts: 4 Rating: (0) |
Ok thanks and excuse me for the confusion. |
Follow us on