9/6/2006 11:39 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (315)
|
Hi Marco, If it is in EPROM then you can't change it online in the CPU 943B of the S5-115U [:(] Then you need a UV-Lamp to clear the EPROM and shoot the EPROM with a PROMMER... [:P] Normally you could put also a RAM-module in to the CPU, it have also some RAM internally, if the programm is not that big, then it could be that the hole program can be placed in the RAM. You might test if the changes are ok and after that clear the EPROM and shoot the program into the EPROM again. Blocks above FB240 are normally system programms for communication and doubleword executions, they are in the internal FW of the CPU, please check the handbook of the 115U for further information S5-115U Programmable Controller [;)] |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on