9/18/2006 11:57 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (150)
|
[quote user="Reuben"] ... I also read somewhere that once you use the GetTagWait function in script that tag is automatically queued at a 1s update (experts please verify!) ... Yes this is true if used in a Global Script. More information is at : http://support.automation.siemens.com/WW/view/en/2952161 As for the original poster's question, why not just log all the data using the Tag Logging system ?? |
9/19/2006 7:30 AM | |
Joined: 5/19/2006 Last visit: 1/11/2024 Posts: 548 Rating: (107) |
[quote user="Reuben"] [quote user="salma"] Now I am confused like never before [8)]: [quote user="Siemens"] My question is: Does GetTagxxxWait register or not a tag for cyclic update from the PLC @ 1sec? The link itself is a bit confusing (to me) like the following statement: Well I don't understand what a picture selection has to do with an action with tag trigger? Here is my understanding regarding Scripts and Get(Set)TagxxxXXX in WinCC: As far as Get(Set)TagxxxXXX I see WinCC external tags like an S7 PLC I/O. Dec |
Last edited by: Dec at: 9/19/2006 7:46 AM |
|
Follow us on