6/30/2010 2:30 PM | |
Posts: 739 Rating: (55)
|
Hello, I´m affraid but it is not possibel to do it with a BOP. With STARTER you can do it, see: |
6/30/2010 3:17 PM | |
Posts: 30 Rating: (0) |
Thanks JensS Yes, with Starter I do it until now. I understand that isn't a way tomake job easier with BOP. bye |
6/30/2010 3:50 PM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating: (477) |
You can use AOP for upload parameters and download it back whenever you required https://www.automation.siemens.com/MCMS/STANDARD-DRIVES/EN/LOW-VOLTAGE-INVERTER/MICROMASTER-4/MICROMASTER-ACCESSORIES/Pages/micromaster-accessories.aspx#AdvancedOperatorPanelAOP |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
6/30/2010 4:41 PM | |
Posts: 739 Rating: (55)
|
Yes of course, you can use a AOP to store, tranfere data sets. But be aware that you have to delete a language in the AOP therefor (and this language can´t be restored!), pls see: http://support.automation.siemens.com/WW/view/en/18473948 |
This contribution was helpful to1 thankful Users |
Follow us on