7/22/2010 7:06 PM | |
Posts: 37 Rating: (0) |
This seems to work, from 0-9 (not the a-fhex extensions),but as I'm still learningI'd welcome any comments..... AttachmentBCD to 7 Seg Conversion Single input.zip (692 Downloads) |
Last edited by: 2700Hp Logo! at: 7/22/2010 7:06 PM |
|
7/22/2010 9:34 PM | |
Joined: 6/20/2010 Last visit: 9/17/2024 Posts: 96 Rating: (0) |
It`s all right, only change the marks (M1,M2....) by outputs |
7/25/2010 5:19 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating: (580)
|
Hi 2700Hp Logo!, please look at the attachment to find an optimized version to convert BCD 0..9 to a7-segment display. It contains only 19 blocks and is a result of the using the logic equations of wikipedia (only present in the german version). The marker s(or outputs) represents the values 0 to 9 and if the value is > 9 constant 9! Atranslation from 0 to F is also possible, but needs more blocks... Best regards Betel _________________________________________________ Perhaps helpful links: AttachmentBCD to 7 Seg Conversion Single input optimized_0_to_9.zip (609 Downloads) |
Last edited by: Betel at: 7/25/2010 5:19 PM==> Meine TAG-Listen: "deut." |
|
7/25/2010 5:41 PM | |
Posts: 37 Rating: (0) |
Thanks Betel. Nice one..... |
Follow us on