9/26/2006 9:55 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (150)
|
What exactly do you mean by faceplate ? Typically a faceplate is configured using picturewindows and tagprefixes. See these FAQs for more info : https://support.automation.siemens.com/WW/llisapi.dll?query=wincc+faceplate&func=cslib.cssearch&content=skm%2Fmain.asp&lang=en&siteid=csius&objaction=cssearch&searchinprim=&nodeid99= If you want to display your bitmaps in WinCC you should copy them into the <project directory> \ GraCS folder, open the PDL and draw a Smart Object -> Graphic Object and link it to your bitmap. I have no idea what are in the CSV files - could be anything! |
9/26/2006 10:59 AM | |
Posts: 87 Rating: (1) |
Dear Salma Thank you very much for the reply. But we are having some prepared WinCC projectin which this faceplates have been already there. But theproblemiswhen we open the graphic editor we can not see the symbols and also they don't show any tag connections. Please see the graphic pdl snap shotwhich shows the current statusofmy problem. In that project directoy there are two faceplate directories one includes bitmap images andsecond one includes *.csv files of faceplates.I am also sending one csv file for the ref. AttachmentAux_Drives.zip (254 Downloads) |
9/26/2006 12:23 PM | |
Posts: 87 Rating: (1) |
HI Thanx for your help once again. Regards Ankur |
9/26/2006 12:28 PM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (150)
|
You're welcome Ankur [:D] Just sorry I couldn't give you a better answer. |
9/26/2006 12:44 PM | |
Posts: 87 Rating: (1) |
Hi Salma I have one more batch file which shows the path on which all bitmap or *csv to be copied. Please have a glance. Attachmentdist_csv_userprop.zip (239 Downloads) |
Follow us on