8/2/2010 10:12 AM | |
Joined: 10/7/2005 Last visit: 4/24/2024 Posts: 3004 Rating: (1046)
|
Hello Yaham the "AWL" instruction is a pure so called Display instruction which does nothing as far as logic execution is concerned (apart from costing youa tiny bit of execution time). Itis merely used to inform Step 5 to automatically display the network in "AWL" when the block is opened. I hope this helps |
Cheers |
|
8/2/2010 10:14 AM | |
Posts: 8 Rating: (0) |
I understood. |
8/2/2010 10:16 AM | |
Posts: 8946 Rating: (999) |
Like fritz allready said, it just will increase the speed of Step5 - editor displaying this sequence. |
Follow us on