8/11/2010 8:28 AM | |
Joined: 10/7/2005 Last visit: 3/28/2024 Posts: 3002 Rating: (1045)
|
Hello Alain Crettaz first of all welcome to the Siemens Forum, let's see if we can help you: You'll probably know already that Strings need to have the maximum String lenght enteredin the first Byte of the String and the actual String lenght in the second Byte (see also Step 7 help for more on teh subject of data type String). Note that these values ought to be decimal values, looking at your VAT however, it appears that you a.) only entered the maximum String lenght (actual lenght is zero) and b.) entered them as character values('2' as an ASCII character equals 50 as a decimal value) I suggest you try the following: Display them as type "Decimal" in the VAT and enter a value of 2 for maximum into the first (maximum String lenght) and second (actual string lenght) Byte of each String. I hope this helps |
Cheers |
|
8/12/2010 8:32 AM | |
Joined: 10/7/2005 Last visit: 3/28/2024 Posts: 3002 Rating: (1045)
|
Hello again Alain Crettaz |
Cheers |
|
This contribution was helpful to1 thankful Users |
Follow us on