8/12/2010 3:55 PM | |
Posts: 13 Rating: (0) |
Dear Miami, We also use T400 board in our factory and I also made an orderT400 dongle( EPDL)from the vendor of our project. I have a demo set and I decided to test those dongles on T400 board. I installed the dongle on a new T400 board (Code: 6DD1606-0AD1). I compiled the software and download the board without any problem. In order to see the error code, Ihave taken out the dongle and download the software againwithout anyerror. Is it normal? What is the exact function of this dongle and how can we understand if there is a problemabout that dongle? Regards. Splitted from Need the order number of T400 dongle EPLD-T39E. |
Last edited by: O_Moderator at: 8/16/2010 7:21 AMnew subject after splitting |
|
8/13/2010 3:41 PM | |
Posts: 13 Rating: (0) |
Hello Miami, In the imported libraries, there are four FB's libraries and one MAKDRA[0711151417 ALL]. I mean, not all of them FB's. |
8/16/2010 12:39 PM | |
Posts: 13 Rating: (0) |
The imported libraries are below: + FBA121 [070806V616 ALL] + FBABAS[071004V616 ALL] + FBSLIB [102200V616 ALL] + FBSSTD [102200V616 STD] + MAKDRA [0711151417 ALL] |
Follow us on