Industry Online Support
Technical Forum
9/22/2010 11:17 PM | |
Joined: 6/4/2008 Last visit: 4/17/2024 Posts: 1481 Rating: (322) |
Hey Amel, I too have struggled with the PID start delay. My PID loop controls pressure brilliantly "ONCE" it starts, butwhen my pump starts with a minimum fixed frequency, there can be from 5 to 30 seconds before the PID becomes active and starts to control the process. This was frustrating, because I had a pump set with a Duty-Assist configuration, and when the duty pump started, the required delivery pressure was not reached in time (about 10 seconds), so the assist pump starts before the Duty pump can accelerate under PID control. I tried many different things, like giving the PID active (P2200) a rising edge from a timer, 1 second after the pump starts. This made no difference. I also wondered if the PID error must be a minimum value before the loop is active, but this also made no difference. I still do not know why this happens. Regards, Graeme Splitted from MM440 Enabling PID after time delay. |
Last edited by: O_Moderator at: 9/28/2010 12:24 PMnew subject after splitting |
|
Follow us on