Industry Online Support
Technical Forum
9/27/2010 9:22 AM | |
Joined: 1/26/2007 Last visit: 4/2/2024 Posts: 123 Rating: (4) |
The hardware used is PLC/TP C7 cpu(3142dp )635 profibus network ... on 2 micromaster 1 M420 and one M440 . The M440 is controling an 22 Kw engine . This engine was damaged the stator cause of bad conctact. The engine was rewound. After rewound , the device is hard start cause sometime get SF+BF (if i am going to diagnostic i get communication error can not read/ write some areas). Also if i am going to slow speed , all the time is stopping (the same error ). i do not thik is bad communication , cause if i succed to start to normal speed , i can work with it 2-3 days witout have any issues . The issues apear only for slow speed , and start. IN attachement i put an diagnostic AttachmentDiagnose.zip (99 Downloads) |
Follow us on