Industry Online Support
Technical Forum
10/13/2010 3:38 PM | |
Posts: 6 Rating: (0) |
I have two OS single stations with pair of CP1613 cardsand redundant 417H CPU in the project (PCS7 7.0 SP3). WinCC data are provided to DCS Honeywell via OPCServer.WinCC. Connection of Simatic and Honeywell networks brings communication errors. To separate both networks,I want to use internal Ethernet port of OS station for this OPCcommunication and NDIS driver of CP1613 cards for the rest (project download, lifebeat monitoring etc.). Is it able to specify different Ethernet ports for this tasks? I have not found any way to do it. Only Simatic Shell specifies the project download path, as I know. I need to have different Ethernet ports for OPCServer.WinCC and for lifebeat monitoring. After activating of NDIS drivers of CP1613 I have problems with incremental project download to redundant OS, that aredescribed in /tf/WW/en/Posts/30534 |
Follow us on