Industry Online Support
Technical Forum
11/17/2010 12:12 AM | |
Posts: 10 Rating: (0) |
We are having a very similar issue on our PCS7 project (7.1 SP1, WinCC HF5). Our issues are happening on activation and de-activation (seems to be an intermittent issue on de-activation)of the WinCC RT. We have a redundant OS pair with RT enabled, and several clients. The issue is with the OS pair. We can download with no worries to each OS and open the project locally through WinCC Explorer. The master OS activates runtime but the standby OS does not and gets stuck while activating the Global Script Runtime (stops at 23% RT). It just hangs there and doesn't time out at all, can only kill the system with a complete power down, not even reset_wincc works!!! Have re-installed PCS7 on the standby OS to no avail, seems like a full system restore is the only option at the moment but would prefer not to have to take this action! Has there been a solution that fixes this issue? I have looked at the event viewer and everything seems to be working correctly, no errors or warnings. Any help would be appreciated! Splitted from Keep getting errors while activating runtim. |
Last edited by: O_Moderator at: 11/17/2010 10:50 AMnew subject after splitting |
|
Follow us on