Industry Online Support
Technical Forum
12/2/2010 5:10 AM | |
Joined: 10/7/2005 Last visit: 5/11/2024 Posts: 3005 Rating: (1047) |
Hello enunes
there sure is presuming you work with the "normal" Step 7 (V5.x),it's called Multi-Instance andthe FAQ below will give you all the detail about its usage(the inbuilt Step 7 help has good info about it too): How do you create and update multiple instances? Just inyou are using an S7 1200 or TIA Portal (you posted in the Step 7 Basic conference which belongs to the TIA Portal),you'll need to reference the following FAQ (Mulit-Instance capability is still limited with TIA Portal V10.5 but will hopefully be just a powerful as it is in Step 7 V5.x when TIA Portal V11 is released): Which function blocks can you call as multi-instance in STEP 7 V10.5? I hope this helps |
Cheers |
|
Follow us on