Industry Online Support
Technical Forum
12/9/2010 4:00 PM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8742 Rating: (1168) |
Dear jirimatus, Let's try to help:
No, you need to order it separately
Perhaps the manual might help: SIWAREX U - Universal weighing module for SIMATIC S7 300 and ET 200M(MLFB 7MH4950-XXXX)
You need the SIWAREX U configuration for SIMATIC S7 (7MH4950-1AK01)
I can not find. Best regards, Wizard |
12/9/2010 4:11 PM | |
Joined: 1/4/2007 Last visit: 9/2/2024 Posts: 1142 Rating: (175)
|
Hello jirimatus, To your questions: 1 - First configuration / commissioning can be done by Siwatool U, but If I buy Siwarex U module, is there also Siwatool U enclosed ? My answer: No. The Siwatool U is not enclosed. Siwatool has the order number: 7MH4950-1AK01. You can download the Siwatool Demo-Version on the following webside: http://support.automation.siemens.com/WW/view/en/10423274 2 - It looks that commissioning can be done also via Step7 ... is it right ? My answer: Yes, but it is more easier to do the commissioning with Siwatool: http://support.automation.siemens.com/WW/view/en/37733600 3 - Where can I get S7 function block "SIWA_U" ? My answer: You can get the S7 function block "SIWA_U" on the following webside: http://support.automation.siemens.com/WW/view/en/28391777 4 - On this forum I found very good Quick guide how to configure Siwarex with Siwatool... is there some manual for configuration (if possible) via Step 7? My answer: Unfortunately there is no manual for configuration via Step 7. Best regards Siwarexi |
Follow us on