1/13/2011 6:05 PM | |
Posts: 9 Rating: (1) |
Hi, In theory it's not possible to use recursive function calls, but here is a st source for recursive functions I just made Basically, by defining a function for each levels of recursion you can do a "recursive" function. And by using some preprocessor pragmas you can save the hassle of rewriting the algorithm over and over again in each level of recursion (so changing the algorithm is fast and easy). With this template you should be able to define your own recursive functions with as many levels of recursionyou need by adding more levels. An inconvenient is that you are limited to as many levels of recursion you defined in the source... Note that I haven't tested it yet because I don't have any Simotion available so please let me know if this thing is working... At least it compiles without error ! Hope this helps ! AttachmentST_RecursiveFunction.zip (240 Downloads) |
Last edited by: mtremblay at: 1/13/2011 7:09 PMRevised algorithm ! |
|
Follow us on