11/1/2006 4:54 PM | |
Posts: 102 Rating: (3) |
Thanks Smurf I have got a field PG but do not know how to format a MMC through it Any help is welcome Thanks and regards Shamsher |
11/5/2006 7:40 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318)
|
[quote user="Shamsher"]Thanks but the problem is that as soon as I insert the MMC card into the CPU slot the stop led starts flashing and if I try to communicate with a normal PC then it says no online partner is active. Hi Shamsher, Please see the pdf for the two possibilitys to delete(format) the MMC. If you have used the MMC in another CPU then it might be a problem, normally you may delete the MMC then in the CPU by holding down the switch onces and after that for 9..11 seconds. AttachmentDelete memory card.pdf (337 Downloads) |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on