5/21/2010 4:16 PM | |
Joined: 10/7/2005 Last visit: 4/26/2024 Posts: 3004 Rating: (1046)
|
Hello PCBuctot first of all, here are some brief answers to your questions, please note that all answers relate to usage of an MMC (i.e. S7 300 usage): 1.) You always and only donwload into the MMC, the OS then automatically "grabs" whaever it needs and copies into its internal RAM (as a matter of fact, you won;t be able to download at all if you do NOT have an MMC in the CPU) 2.)Copy RAM to ROM is NOTapplicable for CPU's with MMC (it can only be used for older type S7 300's with thelarger Flash memory cards). 3.) It does (which makes CPU replacement very easy) 4.) You MUST use a PG or external Siemens USB Prommer (never ever use a "normal"card reader for S7 300 type MMC's) Additional collated detailed info is availble at the links below: S7 300 Memory Cards S7 400 Memory Cards I hope this helps |
Last edited by: fritz at: 5/21/2010 4:21 PMCheers |
|
This contribution was helpful to3 thankful Users |
5/26/2010 4:54 PM | |
Joined: 8/31/2005 Last visit: 3/7/2024 Posts: 2197 Rating: (326)
|
Have a look on this FAQs: S7-300: http://support.automation.siemens.com/WW/view/en/7302326 (read only chapters 1 and 4 in the PDF) S7-400:http://support.automation.siemens.com/WW/view/en/7302549 |
Last edited by: miami at: 1/31/2011 5:24 PMcorrected link Last edited by: miami at: 1/31/2011 5:23 PM |
|
This contribution was helpful to1 thankful Users |
1/31/2011 4:21 PM | |
Posts: 13 Rating: (0) |
Please provide the link to the english version. Thanks. |
Follow us on