10/24/2006 1:12 AM | |
Posts: 6 Rating: (0) |
Anyone know of any incompatabilities or problems between Internet Explorer 7 and WinnCC Flex or Step 7? |
10/24/2006 2:22 PM | |
Posts: 3149 Rating: (171)
|
Hi, I´ve not heard of any problems, but normally I would not install such a "fresh" software on my PC [:D] nemo |
11/7/2006 9:33 AM | |
Joined: 9/28/2005 Last visit: 12/14/2022 Posts: 414 Rating: (28) |
Hi, IE7 is now available as a critical update via microsoft update. If you want to be sure about compatibility problems you should have a look in the different lists available on the support site. Here is a link as an example: Which SIMATIC software packages are compatible with which Microsoft Windows operating system and with STEP7 V5.4? Also lists of winCC and WinCC flexible are available. Normally I wait till one of the update service packages are delivered with new Microsoft software before installing it. I only trust improvements fromMicrosoft if it is tested by Siemens because of the guarantees Siemens gives on working combinations of software. So my advise: don not install IE7, unless you want to test it on one machine. |
Smurf |
|
Follow us on