2/20/2011 1:37 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hi, AMK motor type DV10-31-4-A0F-3000, with following specs. Power 7.5kw Torque 23NMRPM 3000-5500 rpm For this motor you can select 1FK7105-5AF71-1AA0, 8.17Kw, 26Nm, 3000 RPM motor.Please refer the attached sheet for the same. AMK Servo motor type DHS A10-13-155-4-ABF-1500, which has following specs Power 38kwTorque 210NM RPM 700-6000 rpm Attachment1FK7 series servo motor.pdf (921 Downloads) |
Follow us on