Industry Online Support
Technical Forum
11/7/2006 1:35 PM | |
Joined: 5/8/2006 Last visit: 4/29/2024 Posts: 1085 Rating: (77) |
Hi, if you use the ProTool PC Runtime you need only the *.fwd file of the project.The file is creaded when you start theProTool Runtime in ProTool Pro. Then you can copy the file to an USB stick andyou can open the file(like exe-file) on the PC which the project should run. If you use a panel maybe this faq answers your question: http://support.automation.siemens.com/WW/view/de/19109408 Bye |
11/7/2006 1:38 PM | |
Joined: 5/8/2006 Last visit: 4/29/2024 Posts: 1085 Rating: (77) |
FAQ in english: http://support.automation.siemens.com/WW/view/en/19109408 |
Follow us on