Industry Online Support
Technical Forum
3/8/2011 7:12 AM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
Hello, Check there Are the binary input command functions RUN right and RUN left the same on the MM4/SINAMICS G120 as on previous MICROMASTER products? Also look at Operating Instructions: MICROMASTER 420and Parameter List: MICROMASTER 420 Best regards, Hristo Mihalev |
3/9/2011 9:21 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Thread closed, because question is already discussed in the following thread orward and reverse direction of motor of micromaster via din input . Best regards O_Moderator |
Follow us on