Industry Online Support
Technical Forum
3/25/2011 6:14 AM | |
Joined: 6/29/2009 Last visit: 4/16/2024 Posts: 4 Rating: (0) |
Hello there, Im new to the forum but posted this because weexperienced a on this subject matter. We have connected a IM151-7 CPU to the Simoreg on G-SST2. This was working fine in the test set up but was behaving strangely in the final installation. The communicationwillis not re-established after switching of the Simoreg. Switching off IM151-7 CPU doesnt have a problem. To establish communication we need to either change the baud rate in Simoreg to anything and back to correct baud rate. Also disabling and then re-abling the G-SST2 port will do the trick. Later we found that G-SST3 was perfectly working. Communication is established even when you switch on and off Drive and/or IMI51-7 CPU. Does anybody know what the difference is between G-SST3 and G-SST2 and why G-SST2 can not re-establish communication after power off. Both USS ports are set exactly the same. Our test set-up which behaves OK was using G-SST2 but of a newer CUD card than the one we have problem with. Does anybody experience the same problem with G-SST2 and what was done to correct it? Best Regards Splitted from Simoreg 6RA70 Series and USS protocal. |
Last edited by: O_Moderator at: 3/25/2011 10:48 AM |
|
Follow us on