3/12/2011 4:51 PM | |
Posts: 5 Rating: (0) |
Dear Xperts I am using the siemens FM stepdrive 6SN1-227-2ED10_OHAD in smart cards printing machine,but i dont have the manual of above drive for its controling connection. so please provide the technical manual This drive show the output voltage as below UV 80 V VW 78 V & WU 165V Is it drive is OK or Not OK. Splitted from STEP DRIVE 6SN1 227 . |
Last edited by: O_Moderator at: 3/14/2011 9:18 AMnew subject after splitting |
|
3/13/2011 4:26 AM | |
Posts: 2964 Rating: (478)
|
Hello.... What is the error are you facing in the module? Check this document.... http://support.automation.siemens.com/WW/view/en/44453313 Regards, Ekalavya |
Follow us on