5/20/2011 3:32 PM | |
Posts: 739 Rating: (55)
|
Hi, default setting of MM4 is the controling (ON/OFF, Set point) via terminal stripp. If you need to change this, you have to change P0700 und P1000. for further information see parameterlist http://support.automation.siemens.com/WW/view/en/23708204and attachement. For Automatic restart see P1210 Possible Settings: 0 Disabled 1 Trip reset after power on, P1211 disabled 2 Restart after mains blackout, P1211 disabled 3 Restart after mains brownout or fault, P1211 enabled 4 Restart after mains brownout, P1211 enabled 5 Restart after mains blackout and fault, P1211 disabled AttachmentDefault Control Wiring.pdf (246 Downloads) |
This contribution was helpful to1 thankful Users |
5/20/2011 6:09 PM | |
Posts: 7 Rating: (0) |
Many thanks to all of you, now everything is set and working properly, thanks again Best Regards |
This contribution was helpful to2 thankful Users |
Follow us on