5/26/2011 12:30 PM | |
Joined: 9/19/2009 Last visit: 4/19/2024 Posts: 458 Rating: (81) |
Thanks now I can see it. Yes you are rigth! SINAMICS S DXB ----> SI20800E5.GSS the reference ----> 6SL3040-0xA00-0xxx Then I must be wrong because my device is 6SL3040-1xA00-0xxx, So what kind of file GSD do I need? Looking for in internet I found this image. I can see the device SINAMIC S120 CU320 Thanks and sorry for waste your time. |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
5/26/2011 12:52 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
In order to be sure used GSD is correct one, take it frommemory cardof CU there. Under CF card For example in following directory \\SIEMENS\SINAMICS\DATA\CFG\... GSD files depend of type of sinamics, and firmware version. http://support.automation.siemens.com/WW/view/en/49216293 Best regards, Hristo Mihalev |
Last edited by: UMENCHO at: 5/26/2011 12:59 PM |
|
This contribution was helpful to1 thankful Users |
5/26/2011 1:10 PM | |
Joined: 9/19/2009 Last visit: 4/19/2024 Posts: 458 Rating: (81) |
Ok, thanks! But sorry for my ignorance, but I don´t know how I can do it? How I can acces to memory card? is there some FAQs ? thanks again |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
5/26/2011 1:32 PM | |
Joined: 9/19/2009 Last visit: 4/19/2024 Posts: 458 Rating: (81) |
Thanks you very much!!! Best Regards J.Manuel |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
5/26/2011 1:55 PM |
|
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
You are wellcome! |
Follow us on