6/5/2011 7:56 PM | |
Posts: 947 Rating: (45) |
Hello Yes. I make Copy of MMC Card through Card reader. Note! Do not format the MMC card! |
6/6/2011 5:47 PM | |
Posts: 2348 Rating: (263)
|
Ok, i can make test on S7-400, anybody has s7-300 at the moment?) |
6/7/2011 8:51 AM | |
Posts: 8946 Rating: (999) |
I will test. Result soon. |
6/7/2011 12:12 PM | |
Posts: 8946 Rating: (999) |
Here we are. As I said, new (MPI-) parameters on MMC will be used from CPU after insert! After insert new MMC, CPU engaged an overall reset (by it self!). So I have to stop-start again and new parameters are accepted. It makes very sense for me, otherwise how to use a MMC in a new CPU (i.e. after replacement)? I change from 187k5 to 19k2 because CPU don't accept 1M5. See attach. AttachmentMMC_Test.zip (193 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on