6/11/2011 4:43 PM | |
Joined: 4/19/2008 Last visit: 2/9/2024 Posts: 1525 Rating: (159) |
Hi Krsh, You can used the MPI port to Communicate with S7-400 Using the Global Data or X_PUT/X_GET block. Options for communications via MPI In above link you will find the Example also, for Profibus you can used DP-DP coupler DP/DP Coupler is used for the if both the CPU are Profibus master. & easy to configured in the hardware. |
Ammy |
|
6/11/2011 4:45 PM | |
Posts: 241 Rating: (7) |
Him krish, Yes, You can use DP. here is your solution. |
6/11/2011 4:50 PM | |
Joined: 1/28/2009 Last visit: 4/1/2024 Posts: 6836 Rating: (1359) |
Check the following topics: DP link between CPU 315-2DP (slave) and S7-400 (master) with STEP 7 V5.3 Master-slave connection between two CPUs in different projects How do you configure a connection between WinCC flexible Runtime (PC/Panel) and a SIMATIC S7-300/S7400 via PROFIBUS/MPI? Regards |
6/11/2011 4:59 PM | |
Posts: 691 Rating: (36) |
Hey Krish If you don't want to have Master-Slave configuration, you can use GET/PUT Function in S7-400 creating S7-connection in Netpro |
Follow us on