5/28/2011 7:09 PM | |
Posts: 15 Rating: (0) |
Hello The attached file is the zip of source file of FCs and the related FC and DB. QI am getting the output from the FC 26 (as the same is used in all n/w) but after n/w 6 the value is being processed and not showing can anyone tell what would be the possible reason and what is the remedy? What would be my precautions?
AttachmentFC120.zip (71 Downloads) |
5/28/2011 8:01 PM | |
Posts: 89 Rating: (4) |
Attach Symbol table of your project as compiling the source files gives errors |
5/29/2011 9:26 AM | |
Joined: 10/7/2005 Last visit: 4/23/2024 Posts: 3004 Rating: (1046)
|
Hello rahul1234 I wonder if this is purely a display problem when you do online Block Status monitoring as your logic looks alright. Have a look at the link below and see if it fixes the issue: Why does the network status only appear partially during monitoring in the LAD and FBD editor? I hope this helps |
Cheers |
|
This contribution was helpful to4 thankful Users |
6/6/2011 5:28 PM | |
Posts: 691 Rating: (36) |
Hey Rahul Earlier ,Were you getting the values fixed or changing? If changing then Has anybody modified the program? Who else touch that program? There is no question the PLC will produce data itself, unless it has been programmed so. |
6/12/2011 9:10 PM | |
Posts: 15 Rating: (0) |
earlier it was working fine even i checked all last backup and before changing it i compared online with old backup. |
Follow us on