6/11/2011 8:50 PM | |
Posts: 557 Rating: (64) |
hi Can i run Power point presentation(ppt) on winCC run time? Regards |
6/11/2011 9:04 PM | |
Posts: 691 Rating: (36) |
Here is a C Script in WinCC for Excel ProgramExecute("excel.exe"); |
6/11/2011 9:12 PM | |
Posts: 487 Rating: (36) |
Hi sure must be possible , you can start other software via scripts.you can also open a software within a wincc window >have a look at the demo project for wincc on this link Eric |
6/11/2011 9:30 PM | |
Joined: 2/6/2009 Last visit: 3/21/2024 Posts: 938 Rating: (118) |
HI, If you want to open PPT from WinCC runtime, you can use the dynamic dialog Start another application in the graphic designer. If you want to view the PPT in the WinCC runtime screen, you can make the PDF file from the PPT and by using the VB script you can connect it to the WinCC runtime. This is possible by the web browser window object in WinCC. I have attached the VB script namedSetPDFPresentation for your reference and you can call the VB script from you graphics designer as shown below, ( by giing the PDF path under wincc backup) //////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// Sub OnOpen() SetPDFPresentation "V7_New\WinCC_V7_sales_DE.pdf","V7_New\WinCC_V7_sales_EN.pdf" End Sub //////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////// AttachmentDesktop.zip (282 Downloads) |
Last edited by: Saravana kumar at: 6/11/2011 9:45 PM_______________________________________________________________ |
|
6/12/2011 5:46 PM | |
Posts: 291 Rating: (68) |
Hello Eastern, As others have already said, there are so many ways that you can do. Such as the listed below~! As to my recommendation, I would like you to take use of WinCC-Web-Navigator object & hide its "Navigator Title" for playing PPT files. Please refere to the attachment. It's quite easy. just do: 1. Save your .ppt file to a .htm file as shown in the attached video file. This way has an advantage of keeping your animation (macro & so on) of PPT format well. 2. Insert a WinCC-Web-Navigator object into your picture. 3. Let WinCC-Web-Navigator object opens the .htm saved by #1 for you! & hide the WinCC-Web-Navigator's browsing-address so that other doesn't know it's a HTML. Regards, Komi '--------The followings are for your reference only. You don't have to do those ways.------------------ *** Show slide animations during a Web presentation http://office.microsoft.com/en-us/powerpoint-help/show-slide-animations-during-a-web-presentation-HP003081574.aspx?CTT=98 *** PowerPoint 2003/2002 Add-in: Office Animation Runtime http://www.microsoft.com/downloads/en/details.aspx?FamilyID=4033A84A-24C7-40B2-8783-D80ADA33CFF8 *** http://www.microsoft.com/downloads/en/details.aspx?FamilyID=b3f6b934-602d-4a96-9ae9-6583e0ebda9e Some other options: 1. Insert "PowerPoint Web App" into PDL, Let "PowerPoint Web App" play the .ppt for you. http://www.dougamanual.com/blog/217/ http://www.dougamanual.com/blog/217/1246/e5694.html 2. Save .ppt as .html file while editing, insert MS WebNavigator Object into PDL, let "MS WebNavigator" open the .html(.ppt) for you. http://www.imc.tut.ac.jp/course/webct/ppt/ppt.html 3. Use "Google’s answer to PowerPoint" http://www.presentationmagazine.com/googles-answer-to-powerpoint-201.htm 4. Modify the "Open with" registeration of a .ppt file to be Web browser. http://support.microsoft.com/kb/299824/ja 5. Shell execution (For example:) Shell "C:\PROGRA~1\MICROS~2\OFFICE\powerpnt.exe /s C:\temp\test.pps", vbNormalFocus
AttachmentPPT_ToWinCC.zip (291 Downloads) |
This contribution was helpful to2 thankful Users |
6/15/2011 4:08 AM | |
Posts: 291 Rating: (68) |
Hi Eastern, Please fined the attached sample project (built via WinCC V7.0 sp1) for you. In case you couldn't extract a Zip file, please download 7-Zip for extraction. AttachmentEastern_PPT.zip (206 Downloads) |
Follow us on