Industry Online Support
Technical Forum
7/28/2011 7:53 PM | |
Posts: 11 Rating: (0) |
Hi I`m new at Automation, two fast questions: A) I`m pretty sure I need a CF card for CU320-2dp unit to make it work, but just make sure - do I need for 100% CF card to make it work?? B) [snip] ... sorry If i reperat the question but would be appriciated for help, thanks have a good evening.. /tf/WW/en/Posts/60707 ok found out that i NEED a CF card, can I buy one from normal shop and if so, how much capacity i need ??? ok as i read a lto of posts, so I asssume I have to hgave a siemens card also... second question splitted to: cu320 opening hardwareconfiguration from st |
Last edited by: CS Moderator at: 7/31/2011 9:40 AMnew subject after splitting Last edited by: ziro_sub at: 7/28/2011 10:56 PMLast edited by: ziro_sub at: 7/28/2011 9:01 PM |
|
Follow us on