12/1/2006 11:46 AM | |
Joined: 12/1/2006 Last visit: 12/1/2006 Posts: 2 Rating: (0) |
how to connect 0-10 v potentiometer input to which terminals of on boardanalog inputs of CPU 224 XP . |
12/1/2006 11:55 AM | |
Joined: 4/24/2006 Last visit: 4/25/2024 Posts: 8613 Rating: (1147) |
Hi Banjo, Here is a link to manual: http://support.automation.siemens.com/WW/view/en/1109582 See appendix A: CPU specifications and Wire diagrams. Best regards, Wizard |
12/1/2006 1:31 PM | |
Joined: 4/24/2006 Last visit: 4/25/2024 Posts: 8613 Rating: (1147) |
Hi, Connect between M and A+ or B+, that are the inputs. M,I and V are the outputs. Best regards, Wizard |
12/28/2006 4:24 PM | |
Joined: 4/24/2006 Last visit: 4/25/2024 Posts: 8613 Rating: (1147) |
Hello winccipc, The CPU 224XP has just 1 analog output. It can be a voltage or current. Best regards, Wizard |
Follow us on