7/27/2010 2:45 PM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating: (86) |
HI Romulus Well i have changed the "TAG_NAME" to an IO field, but still the tag is not getting trasfred. I have attached the tag name with "D." in the dynamic column, but still no result i have even given in the IO field directly, no result I have attached the customized object for the same. I dont know where i am wrong. AttachmentTEST_1.zip (144 Downloads) |
Jazz |
|
7/27/2010 5:09 PM | |
Joined: 1/4/2010 Last visit: 9/13/2024 Posts: 650 Rating: (40)
|
Hi You have to make a project function for the script. See attachment. So the original function "SSMRTOpenTopFieldEx" works and you get the returnpath and so rest have the right function. I change a view thing: 1) //pch = GetLinkedVariable (lpszPictureName, lpszObjectName, "TAG_NAME");//get tagname pch = GetPropChar(lpszPictureName,lpszObjectName,"TAG_NAME");//Return-Type: char* 2) Be careful that you have a object "TAGNAME" in the picture"@MMS_ANA_MAIN.pdl"! SetPropChar (szPictureReturnPath , "TAGNAME", "Text", szTagName ); I have a "Dtest" in tag managment and a "IOField1" with tag connection "test"in "@MMS_ANA_MAIN.pdl"! Attachmentfct.zip (217 Downloads) |
Last edited by: Romulus at: 7/27/2010 5:12 PMRegards |
|
This contribution was helpful to1 thankful Users |
8/3/2010 12:39 PM | |
Joined: 1/4/2010 Last visit: 9/13/2024 Posts: 650 Rating: (40)
|
Hi Tagolover Idon't know if i understand you right. Do you want to do something like this: /tf/WW/en/Posts/46870#top |
Regards |
|
Follow us on