8/23/2011 7:32 PM | |
Joined: 5/20/2008 Last visit: 3/19/2024 Posts: 2 Rating: (0) |
Hi, i have a problem when I assign an atributte s7_m_c to a structured variable in a DB, I have a limitation in the tag lenght because in the generated tag name the structured name is repeated twice. I have a problem with this because step7 can´t let me to assign this attribute to large structured names because the structured name is repeated twice in the generated tag name. This db is also communicating to a existing HMI Panel so I prefer to not change the lenght of these variables. I would like to know if it's possible to modify the generated tag name as using the variable name only once time instead of twice or use other s7 attributes.
Attachmenttags.zip (71 Downloads) |
Follow us on