Industry Online Support
Technical Forum
7/19/2011 11:22 AM | |
Posts: 89 Rating: (7)
|
Hello, questions: - Do we use Step7 to write logic or WinAC itself is a software to write logic Yes you have to use SIMATIC Manager (Step7) for programming WinAC RTX. It is like a standard PLC. You can also use the WinAC ODK to integrate C-Code. For this the only thing you have to do in WinAC RTX is just call your DLL with ready functions. Then the logic can be implemented in C-code. see: http://support.automation.siemens.com/WW/view/en/35067305 - How robust is the system , can we use it for small engines or turbines control What do you mean with robust? The Microbox works up to +55°C. As an customized version as SIPLUS with extended environmental temperature. Please contact your sales man for this. If you need a smal system then have a look for our new nanobox (IPC 227D): https://www.automation.siemens.com/mcms/pc-based-automation/de/industrie-pc/box-pc/simatic-ipc227d/Seiten/Default.aspx - Is this different from RMOS3 , whats the difference.
It is completely different. WinAC RTX works in a realtime environment "below" Windows (XP, XPembedded or Win7). please see: http://support.automation.siemens.com/WW/view/en/44388946 regards, me |
This contribution was helpful to1 thankful Users |
Follow us on