Industry Online Support
Technical Forum
1/8/2007 4:55 PM | |
Posts: 3149 Rating: (171)
|
Hi, perhaps could using faceplates reduce your engineering time? Please check chapter 3.1 http://support.automation.siemens.com/WW/view/en/18656980 http://support.automation.siemens.com/WW/view/en/21659040 http://support.automation.siemens.com/WW/view/en/24256006 nemo |
1/11/2007 1:15 PM | |
Posts: 3 Rating: (0) |
Thanks for your reply. Wether you use Cut & Paste or Faceplates you still have to enter the tags one at a time. Although the Faceplate allows the tags to be entered somewhat quicker (than cutting and pasting) because all of the properties are visible through the faceplate, it is nowhere near as quick as Tag/Text Substituion would be. One of the links you gave me described a way of changing the visibility of faceplates (FAQ ID:23426415). This doesn't work. https://support.automation.siemens.com/WW/llisapi.dll/23426415?func=ll&objId=23426416&objAction=csView&caller=view&lang=en&siteid=cseus&aktprim=0&extranet=standard I can insert a property but do not get an activation check box, and "Bool" is not available as a data type for the property (4). Animations are NOT visible in the property editor (which is only displayed when the graphics object is selected in the graphic window and NOT when the object is selected in the faceplate configuration window as described in the FAQ) (5). I am running WinCC Flexible 2005 + HF1 on Windows XP Professional SP1. |
1/11/2007 3:36 PM | |
Posts: 3149 Rating: (171)
|
Hi, please install SP1 http://support.automation.siemens.com/WW/view/en/23059737 and then HF6, http://support.automation.siemens.com/WW/view/en/24376196 nemo |
Follow us on