Industry Online Support
Technical Forum
9/21/2011 1:45 PM | |
Joined: 4/29/2010 Last visit: 3/19/2024 Posts: 1557 Rating: (161) |
Hello, flexible can be the client and the WinCC pc can be the server. Take a look at this manual, chapter -> 5.: WinCC flexible Getting Started Options There you can see how you can exchange datas from flexible via OPC. You can check the compatible with WinXP here: With what are SIMATIC WinCC V7.x, V 6.x and V5.x compatible? With what are SIMATIC WinCC flexible 2008, 2007, 2005 and 2004 compatible? Check also this FAQ: Which settings are required in Windows 2000, Windows XP, Windows Vista and WinCC flexible for server-client communication via OPC XML? best regards |
Follow us on