8/2/2011 9:15 PM | |||
Joined: 8/31/2010 Last visit: 9/18/2024 Posts: 1521 Rating: (227) |
Hi Guys, The much awaited SP1 for STEP 7 v11 and WinCC v11 are released for delivery and available for downlload at free of cost. Enjoy Guys Download SP1 forWinCC v11 from here - Service Packs 1 forWinCC V11 to get more info check it out here- Service Pack 1 for WinCC V11 Released for Delivery
|
||
Like it? Rate it! |
|||
8/2/2011 11:53 PM | |
Posts: 2 Rating: (0) |
There appears to be nothing inside the download link? |
8/3/2011 3:57 AM | |
Joined: 8/31/2010 Last visit: 9/18/2024 Posts: 1521 Rating: (227) |
It should be availale there shortly |
Like it? Rate it! |
|
8/3/2011 7:21 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello, For the moment is available only in "DEUTSCH" version of forum. WinCC V11 SP1 link: http://support.automation.siemens.com/WW/view/de/51706933 Unfortunately SP1 supports only 32 bits platform. But with SIMATIC PLCSIM 64 !
Best regards, Hristo MIhalev |
Last edited by: UMENCHO at: 8/3/2011 7:25 AM |
|
8/3/2011 7:59 AM | |
Joined: 8/31/2010 Last visit: 9/18/2024 Posts: 1521 Rating: (227) |
PLCSIM is supported in 32 bit operating systems also or what? |
Like it? Rate it! |
|
9/27/2011 4:39 PM | |
Joined: 8/31/2010 Last visit: 9/18/2024 Posts: 1521 Rating: (227) |
The SP1 for STEP 7 v5.5 and SR1 for STEP 7 Professional 2010 is available here - Service Pace (SP1) for STEP 7 v5.5 / Service Release (SR1) for STEP 7 Professional 2010 |
Like it? Rate it! |
|
Follow us on