10/18/2011 1:59 PM | |
Posts: 23 Rating: (0) |
Hello. I got a problem with software redudanncy. I were trying to connect two redudant 317-2DP PLC to IM153-2 via Profibus, as a redudant link I used Ethernet. And got an I/O error. And couldn't find where it appeared. I've attached project.
AttachmentMinsk_st.zip (115 Downloads) |
10/20/2011 11:25 AM | |
Posts: 23 Rating: (0) |
Hi. So i should update FC 100 arguments in such way, am I right? [code] MB_NO :=200 MB_LEN :=2 [/code] |
10/21/2011 10:17 AM | |
Joined: 10/7/2005 Last visit: 4/23/2024 Posts: 3004 Rating: (1046)
|
Hello ssantiago your are trying to us the CPU's PN port for the redundancy link which is NOT (yet) supported by the Software redundancy package. Have a look at chapter 5.1, 5.2 & 6.7 of the SIMATIC S7-300/S7-400 Software redundancy for SIMATIC S7 manual which explains what Blocks to use for what type of link and what type of S7. The Which modules can you use when implementing software redundancy? FAQ tells you which CP's you can use. Ond once you established the link you may also find THIS Forum post below useful which lists some of the most common pitfalls when using SWR. I hope this helps |
Cheers |
|
10/21/2011 10:56 AM | |
Posts: 23 Rating: (0) |
Thanks, fritz and Tagolover. |
Last edited by: ssantiago at: 10/21/2011 10:57 AM |
|
Follow us on