Industry Online Support
Technical Forum
11/1/2011 2:19 PM | |
Joined: 8/21/2008 Last visit: 8/23/2024 Posts: 141 Rating: (6) |
Dear Wizard,
I used a MMC card of 128kB size. I tried downloading the IP configuration from the HW configutation and also tried using a Primary Setup Tool from a linkhere Even using both the condition, the IP is resetting to 0.0.0.0 after the power Off
No, Since I was new to this controller i thought that the Bus termination module need to be add only if you dont use any IO modules. I am wrong and I now knew that I need to add that bustermination module to clear the I/O error. But what about the IP reset issue? Does it got anything todo with the bus termination module? Pls Help!!! rgds, RBM
|
11/1/2011 2:25 PM | |
Joined: 4/24/2006 Last visit: 9/23/2024 Posts: 8742 Rating: (1168)
|
Hello, I would recommend to use Bustermination module, perhaps it can influence anything. Perhaps an update of Operating System could work. Operating System Updates for IM151-8 PN/DP CPU (6ES7151-8AB01-0AB0) Best regards, Wizard |
Follow us on