11/3/2011 12:40 PM | |
Joined: 10/7/2005 Last visit: 9/24/2024 Posts: 3022 Rating: (1054) |
HelloWilliam B. here's my take on this:
Correct
No, it isn't. OB's that belong to the same priority class will be executed one after the other (i.e.when OB1 is done, the "second" cylic OB's will be called.
Good question and something I wonder myself. Perhaps someone from the TIA Portal development team thought it would be a "cool" idea to allow this (coudl be sold as a "feature" that the classic Step 7/S7 PLC'sdo not have), perhapsit is because IEC61131 does not prohibit, perhaps the answer is as simple as "because you can"etc. etc. Truth be told, I can't think of any good reasons for this, but am open to suggestions.
Dont think so, that is the task of FC's and FB's. I hope this helps |
Cheers |
|
This contribution was helpful to2 thankful Users |
Follow us on