Industry Online Support
Technical Forum
1/20/2007 11:56 AM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (315)
|
Dear Pnachtwey, Please update your STEP7 to the latest V5.3 SP3 or buy a upgrade to V5.4 SP1. [:P] Service Pack 3 for STEP 7 V5.3 and STEP 7 Professional Edition 2004 Also SCL V5.3 is now with a newer SP1 to download and SP2 will come soon. [:o] Service Pack 1 for S7-SCL V5.3 and STEP 7 Professional Edition 2004 I think that after this updates you don't have that trouble anymore. [:P] When you have still the problem then please set your source of SCL on the forum or send a private message with the source to me. [8)] |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
1/23/2007 8:44 AM | |
Joined: 8/31/2005 Last visit: 10/23/2023 Posts: 217 Rating: (40) |
For problems with your license you should contact the Customer Support via a Support Request. On the Support Request form there is a check box called 'Problem with SIMATIC authorization/license' which you have to check. |
Last edited by: Chris at: 1/23/2007 10:42 AMGreetings, Chris |
|
Follow us on