Industry Online Support
Technical Forum
11/13/2011 9:33 PM | |
Posts: 108 Rating: (2) |
Hi Adrian, yeah I actually found that I still had problems with this feature even with update 5. In the end I used the GMsgFunction standard C-script, which is executed every time an alarm message is generated if the "Triggers an action" check box is selected for the message. Refer to the following link for more info: https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=5667814&nodeid4=34677186&load=content&csSort=%2DDOCBETREFF&lang=en&siteid=cseus&aktprim=4&objaction=csview&extranet=standard&viewreg=WW I modified the GMsgFunction so that whenever a message triggers it, a variable in the PLC is SET by WinCC. In the PLC program I immediately RESET the variable and in this way every new message is detected in the PLC. |
11/14/2011 11:40 AM | |
Posts: 1530 Rating: (59)
|
Hello jasonr and other users, it really seems to be this way, that problem isn't completely solved with Update 5. At the moment Siemens is working on Update 6. Please compare german thread, for those who can also read and understand it in german. For all others a short summary: There are still users, which have this unsolved problem, even with update 5. One of them contacted Siemens Customer Support and is now waiting for release of Update 6. My personal opinion is, that there must been something special/some detail by using this feature, this will be the reason why it is sometime solved with Update 5, and sometime unfortunately not, because normally no update will be released without having been tested. As soon as this is available I will post it here. Best regards Bizur |
11/14/2011 1:31 PM | |
Posts: 4 Rating: (0) |
@jasonr, Bizur: thank you for the replies. I think I'll wait for the Update 6 and see what then.
|
11/18/2011 2:55 PM | |
Joined: 8/25/2005 Last visit: 7/5/2024 Posts: 1161 Rating: (110) |
Dear all, Here I found the brandnew information, that the Update you are waiting for is available. Update 6 for WinCC V7.0 SP2 and WinCC V7.0 SP2 ASIAHope with this update everything is working fine! Good luck Sabine |
11/29/2011 11:10 AM | |
Posts: 4 Rating: (0) |
Yeap, Update 6 seems to solve the problem. It is installed for a week now and works flowless. |
This contribution was helpful to1 thankful Users |
Follow us on