11/21/2011 7:56 AM | |
Joined: 3/3/2008 Last visit: 10/5/2023 Posts: 333 Rating: (51) |
hi george, find the attached documents regards ram Attachment611U_s7300.zip (267 Downloads) |
11/21/2011 3:45 PM | |
Posts: 23 Rating: (0) |
Thank's RAM81.A sample program in FBD or LAD because STL in chinese languange for me.Pls help.Best regards |
11/21/2011 4:20 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (713) |
Hello, O.k. one in FBD, now lets hope my Dutch is not like Chinese to you Regards, Marcjan Attachmentservo1.zip (204 Downloads) |
Problem solved? |
|
12/1/2011 12:04 AM | |
Posts: 23 Rating: (0) |
Can anybody help me pls?Thank's |
12/1/2011 7:11 AM | |
Joined: 1/13/2009 Last visit: 2/29/2024 Posts: 19 Rating: (1) |
We have standard functions SFC14 and SFC15 for addressing a slave from a master like s7300.1. Configure the required motor with 611u using simocomu for the required mode—in our case positioning mode.In simatic manager, do the HW configuration for the required CPU and 611u on DP system. Select the required PPO type. Assign the addresses for the selected PPO4. Use Blocks SFC14 and SFC15 for read and write data for transfer of control words5. Refer page 225 for 611u control word details6. Same is available in P9157. Monitoring of the same can be done in Profibus Diagnostics PageStandard cw to be transferred to STW1 isQw280-047E-resetQw280-047F-enabledNote: Also one needs to take care of aspects like referencing, Block transfer with positive trigger,or activate traversing task, Function inhibit bit, Override etc64 blocks can be used for positioning in absolute or relative mode. Sample S7 project attached Regards Syam Attachment611u_rac.zip (226 Downloads) |
12/3/2011 10:32 AM | |
Posts: 23 Rating: (0) |
Thank's Syam for explaination.I don't understand very good STL language.Can you put a sample in FBD or LAD please? Thank's Best regards George
|
Follow us on