Industry Online Support
Technical Forum
12/1/2011 12:00 AM | |
Posts: 2661 Rating: (279)
|
See the following FAQ: What can be the cause of the WinCC error message "More than 10000 actions in work" (up to V6.2: "More than 5000 actions in work")? |
12/1/2011 12:31 PM | |
Posts: 49 Rating: (4) |
thanks for reply
but "SCRIPT,ActionOverflow" isn't because before script said good-bye ? and after all script actions are written to a buffer and then we have "ActionOverflow" on 13:13:12 have "SCRIPT,Thread said good-bye" and next on 13:13:41 "SCRIPT,ActionOverflow:more than 10000 Actions to work" and after "SCRIPT,EndAct Timeout" AttachmentWinCC_Sys_01.zip (103 Downloads) |
12/4/2011 7:21 PM | |
Posts: 49 Rating: (4) |
thanks Jaapie for interesting my problem I think i don't have a lot of action, but i have 4 monitors, block icons was modificated and i calculated in C action diffrent between SP and PV I do sam test. Copy dynamic element from 4 the most often opening pictures and put it on one screen and next open this picture on 4 monitors, and try to open faceplate. Everything goes down, faceplate opening few minut. After sam time i have "SCRIPT,ActionOverflow:more than 10000 Actions to work" This test goes 4 houer i have few ActionOverflow but no "SCRIPT,Thread said good-bye" so i thinks ActionOverflow don't crash script.exe Ok visualisation goes slowly .... very slowly, but work anyway, and after changed pictur on monitor, visualisation work normaly (without restarting wincc RT or computer) So what coused "SCRIPT,Thread said good-bye" ? |
Follow us on