Industry Online Support
Technical Forum
12/19/2011 10:36 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
It should be possible as http://support.automation.siemens.com/WW/view/en/41928929
Best regards, Hristo Mihalev |
12/19/2011 10:41 AM | |
Joined: 1/26/2011 Last visit: 8/11/2022 Posts: 243 Rating: (67) |
Hi codeexpert, which version of Windows 7 do you have? regards |
12/19/2011 10:55 AM | |
Posts: 31 Rating: (0) |
Win 7 Ultimate 32 bits SP1. thank you for your interest. |
Last edited by: codeexpert at: 12/19/2011 10:58 AM |
|
12/19/2011 11:21 AM | |
Joined: 1/26/2011 Last visit: 8/11/2022 Posts: 243 Rating: (67) |
Hi codeexpert, maybe the problem is the SP1 of Windows 7. in the following FAQ there is a list of the compatibility. And the is no entry of Windows 7 SP1. I'm not quite sure but may can be the problem. http://support.automation.siemens.com/WW/view/de/8675614 You can try to uninstall the SP1 and look if it works. Do you have installed other Siemens software? regards |
12/19/2011 11:33 AM | |
Posts: 31 Rating: (0) |
hi bigfoot, i have also WinCC 7.0 SP1 installed on OS and functioning well with no problem. I will check out the link. Thanks and regards. |
Follow us on